This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC25660: 1000W AC/DC system using a PFC UCC28180 + LLC UCC256601

Part Number: UCC25660


Tool/software:

HI TI team,

The design specifications are Vout = 40V, with a typical output of 360W and a peak output of 1000W (1 second on, 3 seconds off, controlled by a secondary-side MCU).

We encountered an issue where the load power could not increase. To address this, we adjusted the RISNS value from 200 ohms to 110 ohms, which allowed the load to increase to 800W. However, with this RISNS value, when returning to a 360W load, the MOSFETs in the LLC circuit became unstable and overheated.

Since we only require a stable output of 360W, what other methods can be used to adjust the power limit for protection without changing the RISNS valu?(Possibility of entering a dead zone)

Attach the circuit diagram.

sch_adp1000a_e20_20241009.pdf

thanks & regard 

Noah

  • Hi Noah,

    TSET, ISNS, BLK resistor values influences the FBReplica magnitude for a given power. You can tune these values in the design calculator to see the variation in FBReplica vs power.

    Let me know if you have any further questions.

    Regards

    Manikanta P