Tool/software:
Dear TI engineers,
I would like to know how much large inductance I can use for stable operation.
For example, if Vin = 10.8V-13.2V, Vout = 8V to 10V and ILED=500mA, I would like to know the maximum value of inductance for stable operation to suppress LED ripple current.
If I use 33uH, does DC/DC converter will work well?
I know KIND might be little bit small in above case, but I think there is a chance to work well inspite of some undesirable jitter caused by small VFB ripple.
If there is some critical criteria for chosing large inductance, would you kindly let me know it?
Thanks and best regards,
YTK