Tool/software:
Hi team,
If I want to use OVP and UVP with the default values (OVP=32.6V, UVP=14.9V), is it correct to set R3=0Ω, R1=0Ω, and R2=open?
Should R2 have a set value?
Also, if I want to use OVP with the default settings and not use UVP (keeping it as low as possible), would it be acceptable to set R3=0Ω, R1=820kΩ (for example), and R2=open?
Should R2 have a set value?