This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27426: Gauge enable and status update

Part Number: BQ27426
Other Parts Discussed in Thread: BQ27Z561,

Tool/software:

Hi team, 

1. In BQ27Z561 or latest device, customer need to set Gauge_Enable to start Gauging algorithm. 

Bu I did not see this in BQ27426, Does this socket need to do this?

2. In TRM, status 00 means there are limits in Qmax and Ra update. 11 means no limit(after golden learning).

It was strange! I think there should no limit during golden learning(default should be 11). And after learning, there should be limit(00). 

Is that typo error?