Other Parts Discussed in Thread: BQ79600-Q1
Tool/software:
Dear Team,
Bq79600 is used communication with 15 pieces bq79718 and 1 piece bq79731. All ICs are connected to with daisy chain. Sometime happens to communication fault. The fault is 79600 doesn't communie with both bq79731 and 79718. It should be noted that this fault does not occur consistently; it may manifest on the 50th or 40th attempt. Bq79731 and Bq79718 doesn't response in a time. While the problem is solved by itself, sometimes it requires turning on and off.
We analyzed the fault. I can share more detail about the fault. BQ79600-Q1 is used to communication with Bq79718 and Bq79731. In the below picture everything works well. Yellow is power(IC power), green is daisy chain communication, blue is Rx pin of MCU and is connected Bq79600, purple is Tx pin of MCU and is connected to bq79600.

If the fault is occured, signal is changed like below picture. Tx is transmitted the data but Rx doesn’t response. During this time daisy chain communication is fault. MCU can not communication with Bq79718 and Bq79731. In this state bq79600 doesn't send fault summary. Bq79600's nfault pin is normal.

What could be the reason for this fault? Could you help this issue? Thanks for support.