Part Number: LM25183
Tool/software:
Hi team,
There is no problem with the current application of LM25183, but I have questions about the selection of Schottky diodes. Could you please help me answer them?
1: For DF and DFLY, the diode I chose is LRC's S-LMBR1100FT1G: Diode Schottky 100 V 1A
Is the rated current of 1A sufficient for the application? What is the basis for determining the rated current parameters of the diodes in the two positions?
2: For the flyback converter quickstart tool, does the peak current represent the peak current of the primary and secondary coils of the transformer?

BR,
Ethan