Tool/software:
Good Morning,
I contact you to have some information about the LMZ14203 behaviour in short-circuit.
We impleted this component to generate two output voltage level : a 3V3 and a 5V from a single supply in range [8V;30V].
Schematic 5V :
Schematic 3V3:
In our short-circuit test, we checked the current waveform on the output.
We were surprised to see different behaviour between the 5V output and the 3V3 output.
Here are the oscilloscope screen :
P5V : (Voltage in blue and current in purple)
We though that this screen is a good functionning with low output voltage and some repetitively low current spike which mean the component try to check if the Short-circuit is still present.
P3V3 (in green voltage and in purple Current):
On this test, we see large current spike with remaining voltage.
In fact, we don't see it on this screenshot but the first spike seems to have the same behaviour as with the P5V.
All the following spikes are like the figure above.
During this test, the Input voltage of the component is stable. Same configuration of test are used for both capture above, a direct short circuit.
We wanted to ask you if you have an idea why this behaviour happened ?
How is managed the shortcircuit protection ?
Thank you for your help,
With best regards,
Olivier EMANUELY