Tool/software:
I would like to inquire about the defect while using LM5160A.
The circuit diagram is as follows and the output waveform of the defective B/D is as follows.
If 10V is forced from the outside after deleting diode D517 for this defect, the IC will operate normally again.
Therefore, it is assumed that the internal VCC regulator is defective.
Can you explain the mechanism of the defect??