This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi team,
Q1. Datasheet p11 shows "Limit the current into the power-good flag pin to less than 5 mA D.C." Will this IC be damaged if this is not observed?
Q2. The PG pin (#4) is an open-drain pin, but is it OK to use an empty pin when not in use? Or is it the right thing to drop it on the GND?
If we look at p1 or p4, we can interpret it as OK with an empty pin.
However, if we look at P11, it is written that it should be dropped on the ground.
From datasheet:
p1: In Simplified Schematic, the PG pin (#4) is empty.
p4: "Open drain power good flag output. Connect to suitable voltage supply through a current limiting resistor.
High = power OK, low = power bad. Flag pulls low when EN = Low. Can be open or grounded when not used."

p11: "If this function is not needed, the PG pin should be grounded."
Regards,
Hiromu
Hello
The device will not be damaged if more than 5mA is used in the PG flag.
The PG flag can either be left open or grounded when not in use.
Thanks
Hi Stasi,
Thank you for your comments.
Could you tell me more details about why we can left PG flag open without following this?:
p11: "If this function is not needed, the PG pin should be grounded."
Regards,
Hiromu
Hello
It is only a recommendation to ground or to leave open.
Both ways are acceptable.
Thanks