This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi!
I am in design stage and now I use TPS48xx for 24v 15A loads (80V max expected).
I would prefer integrated solution, and I see that TPS1685 may be this solution.
It would not switch fast, I expect from switch basically switching and OC protection with I monitor and fault output.
Here is my TPS48xx based solution:
As you see pretty much components I would like to evade, especially because I have 4 channels like this (not parallel, independent)
And with TPS1685 it looks like solution will look much smaller with all functions I basically need:
What do you think about it?
Or there is some change between eFuse and high-side switch that I don't understand?
Thanks!
Stas
Hi Stas,
You are right. TPS1685 eFuse will be a good fit here.
Regards
Kunal Goel