This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
I have a technical question regarding EMC testing for a PoE design using the TPS23730EVM-093 evaluation module.
In my setup, power and data are delivered to the evaluation board via an Ethernet cable from a PoE injector. I have modified the TPS23730EVM-093 board to provide 60W at the output.
I am preparing for EMC tests, specifically surge and burst tests, and would like to understand the correct testing approach in this scenario:
Your guidance on the correct procedure would be greatly appreciated.
Hi David,
Thanks for reaching out!
I am currently working on verification. Will be back for E2E support from Jan 20th. Thanks for your patience.
Best regards,
Diang
Hi David,
You may need to connect to a LISN or other specific tester for EMC testing. The test procedure normally depends on the product's standard while PoE standard does not have a specific requirement for EMC for now.
For testing more information can be found in https://www.ti.com/lit/an/slua469/slua469.pdf which is an application note including test example.
Besides, PMP23287 is 24V output version using TPS23730.
Best regards,
Diang