This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23730EVM-093: urge/Burst Testing for PoE Design with TPS23730EVM-093

Part Number: TPS23730EVM-093
Other Parts Discussed in Thread: TPS23730

Tool/software:

Hello,

I have a technical question regarding EMC testing for a PoE design using the TPS23730EVM-093 evaluation module.

In my setup, power and data are delivered to the evaluation board via an Ethernet cable from a PoE injector. I have modified the TPS23730EVM-093 board to provide 60W at the output.

I am preparing for EMC tests, specifically surge and burst tests, and would like to understand the correct testing approach in this scenario:

  1. Should the 24V output be tested directly for surge/burst immunity?
  2. Or should I only test the shield of the Ethernet cable?

Your guidance on the correct procedure would be greatly appreciated.