Tool/software:
Thanks for the answer.
Question 1.
I understand that there is a V-reading error problem with Ra=V-OCV(DOD,T)/I.
But the answer to question 2.
>Since voltage readings are not accurate, SOH and Ra table values should be disregarded.
I don't think this explanation explains the phenomenon where SOH worsens at low charge/discharge cycle numbers and then returns to normal as the number of cycles increases. Because if the voltage readings are not accurate, then wouldn't the Ra table be disregarded at low cycle numbers? I think this is a good idea.
Could you please explain?