This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25185: Battery Charging circuit

Part Number: BQ25185

Tool/software:

Hello, I need to confirm that my design for charging a 3.7V battery is correct. My question is: since I’m not using the TS option, is it correct to tie the TS pin to ground with a 10k resistor?

  • Stil waiting for a reply it's urgent please

  • Hello Firas,

    Yes, if the TS function is not being used, the TS/MR pin should be tied to ground with a 10k.

    Best regards,

    Alec Lehman

  • "Thanks for replying. My last question: Is my usage of STAT1 and STAT2 correct, since there is no example provided in the datasheet? If you notice anything that could prevent the battery from charging when VIN has a 4.7V input, please let me know.

  • Hello Firas,

    STAT1 and STAT2 are open drain status outputs which can be connected to either an LED or an I/O pin of an MCU to inform the user or host about the charger status. If these pins are not required in your design, they can be left floating.

    You can refer to the BQ25185 EVM schematic, which can be found in the EVM User's Guide: BQ25185 EVM User's Guide

    From your schematic, it appears that D6 and D7 are not LEDs. If you intend to use LEDs, ensure you select appropriate current-limiting resistors.

    Lastly, since you are using a 5k on the ILIM/VSET pin, VBATREG will be set to 3.65V. This means your battery will not charge up to 3.7V, so please ensure this aligns with your requirements.

    Best regards,

    Alec Lehman