Tool/software:
Hi,
So I asked this question yesterday, but the thread is now locked. There is conflicting information on the E2E page, so I cannot draw a concrete conclusion.
In these 3 posts Mike O' states this is not possible in links (1) and (2). However in the link (3) Colin Gillmor states this is possible.
Link (1) and (2) coincide with what other documentation says that the switching pattern must match the primary side as stated in other TI resources using external logic by AND'ing A and D and AND'ing B and C, but I need more clarification. Why can the secondary not short circuit when gate signals E and F overlap as they would in a Center Tapped configuration. The center tap configuration during the freewheeling period shorts both FETs causing a shorted secondary and (0.5*Inductor current) flowing through each MOSFET. During freewheeling period PSFB there will be no primary winding power delivery and the Power transformer will be short circuited on the Primary side. So why would having a short circuit secondary winding matter during the Freewheeling diode period?
Regards,
-Noah