Other Parts Discussed in Thread: BQSTUDIO, BQ25756EVM,
Tool/software:
Hi, I just bought EV2400 on digikey, connected it to a computer on win11, but I couldn't update it with the EV2400_Updater_v0032.exe utility (Error: No Free EV2400s Detected.), with the -s flag the program opens and immediately closes. BQSTUDIO also doesn't detect the EV2400 connection, neither when it's alone, nor when it's connected to a working BQ25756EVM.
In the computer, the device manager detects it as a hid compliant vendor defined device and USB input device (two devices at the same time).
It doesn't respond to the reset button (which is on the device)
All three LEDs are constantly on all the time.
I checked it on two different computers with win11, the behavior is absolutely the same.
What could be the problem?