This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24040: Pre-termination floating?

Part Number: BQ24040


Tool/software:

I'm trying to select a Preterm resistor value for my application.

I can see in the datasheet that 2k is the value for 10% termination current and 20% pre-charge current.

I also see a note that the same configuration is achieved if the Preterm pin is left floating.

Is this accurate that the same operation is achieved if the pin is left floating or a 2k resistor is applied?