Other Parts Discussed in Thread: TPS65219, , USB2ANY
Tool/software:
Hello,
I am using TPS65219 EVM-SKT, and I am using the standalone TPS65219 Gui for windows. Below are the steps I go thru, but the new address does not get saved.
When Gui connects to EVM-SKT, I press the EN_PB , and I2C address is 0x30 ( Addr 0x26 , 0x30 ). On the Register Map of the Gui, I select "Deferred Write", and for addr 0x26 I input 31, and for addr 0x34 I input (Custom Program CMD in the drop down ) 0x0A. Then I click on Write All Registers. The Gui loses connection to EVM-SKT. After recycling power, the gui connects but the address is 0x30.
Or I do the same above process from initialized state with the same results.
Please provide step by step instructions for changing the I2C address as I am planning to use two TPS6521905 devices.
Thank You.