Other Parts Discussed in Thread: LMR60410, TPSM33615, ,
Tool/software:
Hi support team,
When the output voltage is 8V and the input voltage is 9.5V, the PFM operation switches to PWM operation.
This causes the input current to increase from 400uA (in PFM) to 5mA (in PWM).
(The load current is expected to be extremely small.)
If the input voltage is 9.6V, it remains in PFM and maintains 400uA.
The LMZM23601SILR does not allow adjustment of the internal frequency, so I don't think it is possible to adjust the inductor valley current.
Therefore, I think it is impossible to control the switching between PFM and PWM.
I am looking for a way to maintain PFM.
To control the switching between PFM and PWM, is it necessary to choose the TPSM33615RDNR, which allows internal frequency adjustment, or the LMR60410 with an external inductor?
Regards,
Dice-K