Other Parts Discussed in Thread: TXH0137D,
Tool/software:
Hello
In one of my new designs, I chose TXH0137D for driving some FO's and Relays.
Unfortunately, it is not available anywhere.
I want to see if TPL7407LA can be used?
I chose the former because of its lower tpd 250 nS against 350 nS of the latter
and also because the FO's are driven from +5V while the Relays are driven from +24V.
I can compromise with the 350 nS of the Prop delay but can I use different driving voltages
like +24 V for Relays, 4 Channels while driving FO's from +5V, 3 channels?
Without having to change the Relay coils to +5V can I use the TPL7407LA directly?
Thanks