Part Number: CD40109B
Other Parts Discussed in Thread: UCC44273, UCC27517, TXH0137D-Q1, CD4504B, TXH0137D,
This is reg translating a 3.3 V PWM Signal to +15 V levels with approx 5 mA Source & Sink
CD4504 Data Sheet is not guaranteeing this translation .
Some one from TI ( in some earlier threads ) had recommended CD40109 with Vcc as 3.3 V and Vdd as 15 V
and applying the 3.3 V DSP PWM Signals to the 3.3 V Side.
While studying the Data sheet of CD40109 , this Fig No 10, High Level Supply Voltage Vs Low Level Supply Voltage,
the recommended Domain is not a perfect Rectangle but the Left vertical line appears slanted.
Essentially for a 15 V along the vertical axis, where this slanted line intersects and I drop it to the Horizontal axis
does it guarantee 3.3 V , is my Question.
If I recall, ( though not sure ) even CD4504 has a similar slanted line.
Would someone be good enough to clarify?
Thanks and regards
Varun