This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: Current Scaling to support 100A current

Part Number: BQ40Z80


Tool/software:

Hello, 
I got to know that the scaling must be done to increase the current capability, as the battery i am using has 8.4Ah as design capacity the scaling factor is 0, but according to current requirements the current scaling factor is 100/32.767 = 3. I changed the scaling factor to 3 and updated the protections part.
In design capacity both mAh and cWh, should it be same or should I change it as the current scaling factor is increased ?