Other Parts Discussed in Thread: TPS25751
Tool/software:
We are using the PD controller TPS25751 and the charger IC BQ25798. Our goal is to fast-charge the battery using the PD controller and charger IC. The USB 5V will come to the PD controller and then go to the battery charger IC .We are using a dual-input circuit for the battery charger IC. The outputs of the battery charger IC are the PMID and SYS pins. Out of these, which pin's output should we provide to our system load?