Tool/software:
Hi team,
When this device is operated below condition. It is observed that the current consumption increase up to about 10mA in a cycle of about 20 ms.
・Using EVM circuit
・Vin=1.5V
・Vout=3.1V
・No load
I guess this is because of Burst mode operation when light load and the reason of this cycle(20ms) is that it takes time to dicrease output voltage to Vout_bst.
Is my understanding correct?
Please your opinion.
Best regards,
teritama