This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I am using this part to power AM3358BZCZA100 processor (Taking reference from Bealgebone)
My power input configuration is:
1. 5V input from DC supply.
2. No battery
3. No USB power
Is the schematic correct for this input configuration. Specifically, should I connect the 5V DC input to AC pin or to the USB pin?
Hi Mohit,
Thank you for reaching out on E2E. The TPS65217x Schematic Checklist should be a helpful resource in your designing process.
Since you are using the 5V DC input only, this should be connected to the AC pin. And the USB pin should be grounded.
Please also see the following comments regarding the schematic:
Let me know if you have any further questions or comments.
Best Regards,
Sarah