Tool/software:
I have built a boost converter with the below specifications for charging a battery pack. It works as expected with a resistive load, regulating to 72V at lighter loads and limiting input current (thus reducing voltage) at lower resistances. Scoped waveforms look good in these conditions. However, when I attach the output to a battery pack, the IC becomes damaged as soon as switching would have begun. I brought up the input voltage slowly, once UVLO was >0.4V, the Vcc regulator turns on and works correctly, however, as soon as UVLO exceeds UV threshold, the IC is instantly fried.
I assume the difference in behavior is related to the pre-biased load but I can't figure out the exact issue. My understanding is that based on the schematics included below, the LM5122 should be operating in diode-emulation mode with hiccup mode turned off, therefore, there should be no reverse current through the high-side switch. R14 is placed, grounding MODE pin. Please ignore R15 which is DNP on the board, just present to provide an option for using FPWM mode. I do have a snubber on the high-side switch. Inductor saturation current is rated several times what the inductor current limit is. I'm not sure if perhaps this is an issue with soft-start or the LM5122 IC sinking current for some reason. I don't believe there is damage sustained to either FETs or the various control components. The batteries have a 5A current fuse that is intact.
Is there anything the LM5122 is doing due to the initial conditions of the battery load voltage that could be causing this damage? If so, how can I alter the circuit to prevent it? Any help is appreciated.
Vin: 50V
Vout: 70V
Rsense: 20 mOhm (should limit peak inductor current to 3.75A)
fsw: 150 kHz
L: 47 uH