Other Parts Discussed in Thread: AMC3302, , PMP22339
Tool/software:
I am designing a flyback converter and would like for the control loop to primarily regulate a constant output current to a pre-biased load bus. Therefore, my design idea is to place a sense resistor between the converter output and the load, sense the drop across this resistor with an isolated differential amplifier (to maintain isolation across the flyback, such as the AMC3302), and feed this voltage back to the feedback pin of the LM5156 using a voltage divider to tune the desired setpoint and an op-amp to make the differential output single-ended.
I have a few questions based on this:
1. Are there any obvious issues with this design idea?
2. Perhaps there is a better IC for this application? I am aware that there exist some CC/CV PSR ICs, but this design seems like it would generate more accurate regulation at light load and eliminate the need for an auxiliary winding on the flyback transformer.
3. Is there a way to combine the ACM control loop with a voltage control loop that shuts off the converter in the case of overvoltage on the output?
3. Why does the LM5156 datasheet show the compensator components connected from COMP to GND rather than COMP to FB as I am accustomed to seeing?
Thanks for any help that can be provided.