This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25947: TPS25947

Part Number: TPS25947


Tool/software:

Hi All.

i would like to connect two TPS259474ARPW in parallel in order to reduce the overall series resistor Rds on each item (two resistors in parallel) , the two items will get the same p[ower supply and will drive the same voltage to the board loads, thus producing half the Rds in series to the loads, theoretically. 

1.is it possible to do so with the items, there is an example on pages 44-46 showing similar set-up. i would like to be clear, the power in and power out will be the same on the required configuration. 

2.does this configuration will actually drop the total Rds to the loads, or does it work's differently inside the TPS259474?

please clarify on all the required info.

Thx.

NItsan.