This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21551-Q1: Regarding the Power Estimation

Part Number: UCC21551-Q1

Tool/software:

Hi Expert,

We are estimating the power for the driver using the equations from the UCC21551-Q1 datasheet, including a 50% tolerance. We are employing a Negative Bias with a Zener Diode on the Iso-Bias Power Supply Output for both the HS and LS sides of the driver. From the power calculation, power requirement is 0.76W for each drive (HS and LS). However, our simulation shows 1.3W for the HS side alone. Could you help us resolve this discrepancy?

Parameters:

  • VDD: 24V
  • QG: 7.94E-08C
  • Fsw: 200,000Hz
  • PGSW: 0.76224W

    Thanks and Regards
    Unnimaya V