This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ77216: BQ76952 with BQ77216 for UL1973 Compliance with no Safety Critical Software

Part Number: BQ77216
Other Parts Discussed in Thread: BQ76952,

Tool/software:

I am looking to use the BQ76952 battery monitor to create a HW architecture for a low cost 48V battery BMS that complies with the latest UL1973 certification requirements that, critically, does not require any safety-critical software. Will using the BQ77216 as a secondary protector suffice? The goal would be to have a non-functionally safe MCU that primarily communicates with CAN/bluetooth devices. 

Can you provide recommendations or reference materials on compliant architectures? Is there a TI representative I could get in touch with directly?