This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-R2: Start of charge for learning cycle.

Part Number: BQ34Z100-R2


Tool/software:

Hi, I have a quick question that might be the cause of my issues with the learning cycle. In the documentation, it says: "...If VOK is never set, this means that it did not start with an empty battery..." Does "empty battery" mean starting with 0% SOC? I’m using a lead-acid battery for the learning cycle, and with these batteries, after discharging them to 0%, they increase in voltage when they relax. How should I handle this? Do I really need to start the charge in 0% SOC after relax for VOK to be set? Thanks.