Tool/software:
To whom it may concern:
We are using BQ78Z100 for a single cell battery, and noticed the fuel gauge can't get into SHUTDOWN mode when the cell voltage is lower than the SHUTDOWN threshold (2.5V), even Vpack (3V) < Charger Present Threshold (3300mV).
This special design could have 3V on the P+ terminal, but the battery is not charging (current = 0). Based on the BQ78Z100 tech reference, it should meet the voltage base shutdown conditions, but based on our test, the fuel gauge can't fall into SHUTDOWN mode. We also tried to increase the Charger Present Voltage to 3.6V, but it still didn't help.
Status Condition Action
Enable Min cell voltage < Shutdown Voltage OperationStatus()[SDV] = 1
Trip Min cell voltage continuous < Shutdown Voltage for Shutdown Time Turn DSG FET off
Shutdown Voltage at PACK terminal < Charger Present Threshold AND Current() ≤ 0 Send device into SHUTDOWN mode
Could you help to check?
Thank you!
Chen