This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: Max error 100%, FCC value not updated

Part Number: BQ4050
Other Parts Discussed in Thread: GPCCEDV

Tool/software:

HI TI Engineer:

We made a batch of batteries, but during the aging learning process of the production line, only a few batteries made multiple cycles, and Max error 100% and FCC values could not be updated, which means that the learning failed. There are LOG and GG files attached, please help analyze the data.

The actual capacity of the battery is OK, why in a batch of batteries, only a few batteries can not learn successfully?

BQ4050 Maxerror 100% dis-log.xlsxBQ4050-GG-20250113.gg.csv