Tool/software:
Helo:
We are going to use this chip for converting 30V to 100V for a 200W converter.
Isolated.
What other flyback chips can you suggest?
Also: what chip will give us a feeback loop of high bandwidth so that we can adjust the output voltage well within 10 usec! Once a load pulse has started with a trigger, the sensed load current has to be fedback so that the output current in the load remains constant. Well, it sounds like we are making a constant current source but the current load lasts only for 500 usec. In order to keep the load current constant during the pulse, should the feedback not be fast?
We might use a battery charger - because we have 30 mF capacitor bank. This has to be charged to 120V. Which is then discharged by 400A over 500usec. At a rate of 40 Hz.
What battery charger can operate in a bosst mode?
appreciate any discussion on this topic.
r