This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A33: VREF Vs temperature clarifications for TPS7A33.

Part Number: TPS7A33

Tool/software:

Hello Sarah/ TI support,

We are using TPS7A3301.

1. The limits for VREF at 25'C are specified from -1.192V to -1.157V. Does this include manufacturing, other variations at 25'C?

2. Fig-1 has temperature variations but again those doesn't match with limits given in datasheet. So now question is what are limits over temperature considering manufacturing, other variations?

3. Is this correct in fig-1 that shift at 85'C is more than 125'C..? 

Regards,

jagdish