LM5146: LM5146

Part Number: LM5146

Tool/software:

50V to 28V CONVERTER

I have designed a buck converter utilizing the LM5146RGYR. However, I'm encountering an issue with excessive heat generation on the board, even when operating without a load. The test conditions are 50V input and a 28V 15A output configuration.
I would greatly appreciate any assistance or insights you may have regarding this issue.
Thank you for your time and consideration.
  • Hi Aarindom,

    Please fill in the quick start calculator here ( https://www.ti.com/tool/LM5145DESIGN-CALC) and share with me. 

    Thanks,

    Best Regards,

    Taru

  • I have updated the value according to the calculator, but I'm still encountering excessive heat and an output voltage of only 14V instead of the expected 28V. Additionally, the output voltage is slowly increasing, and the temperature is rising simultaneously, without a load.
    Could you please advise on how to resolve these issues?
  • please find the data from the calculator

  • Hi Aarindom,

    Can you probe the switch node, inductor current and output voltage, 

    Furthermore, can you test without populating the filters at the output? 

    I also see some discrepancy in the values that you have filled in the quick start calculator v/s the schematic:

    1. Output caps - you have mentioned 200uF - I only see 30uF in the schematic - that too will be derated at DC Bias. Also, ensure they are rated at ~2x the nominal output voltage.  

    2. Inductor - Schematic - 10uH - Calculator = 3.3uH? 

    3. ILIM- Schematic says 1.58k (quick start says 110 Ohm). 


    Please fill in the calculator accurately and share the excel sheet here. Also, share the most updated schematic with me. 

    Thanks,

    Best Regards,

    Taru