Other Parts Discussed in Thread: BQ34Z100-G1, BQSTUDIO
Tool/software:
Dear Team,
I have a question regarding the 76952 registers and would appreciate your support.
Our current design utilizes the BQ76952 and BQ34Z100-G1 for a battery pack consisting of 15 series LiFePO4 cells. The TS2 pin of the BQ76952 is used to wake the IC from shutdown mode via a button. However, when the PCB is initially energized, the IC automatically wakes up, and the button does not function as expected. This means that every time the battery pack is mounted or dismounted, the IC remains in the wake state.
If the shutdown command is sent via BQStudio, the IC enters shutdown mode. In this condition, the IC remains in shutdown mode regardless of whether the battery pack is mounted or dismounted. The button is only functional in this state, allowing the IC to wake from shutdown mode.
I would like to configure the system so that the IC always wakes from shutdown mode using the button, while also ensuring that the IC enters shutdown mode when there is no energy(battery pack). How can this be achieved?
Thank you for your support.