This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25750EVM: 0.1uF capacitor line items

Part Number: BQ25750EVM

Tool/software:

Hi,

C12 and C18 are rated for 25V. Is there any specific reason for 25V? Because C10 is also 0.1uF and rated for 100V. Is it fine to use 100V part number at C12 and C18? Please check and confirm.

Regards,

Saravana

  • Hello Saravana,

    Yes, you can use 100V rated capacitors for C12 and C18.

    C10 is rated to be 100V because it can be exposed to up to 80V during normal operation.

    C12 and C18 are only exposed to the voltage between BTST and SW. The max allowable voltage here is 14V.

    Best regards,
    Ethan Galloway