Tool/software:
Dear TI experts,
My customer considers UCC21551CQDWKRQ1 for their new project.
And my customer has few questiona about it. Could you check the questions below?
1. About DT (Deadtime) pin
In the red area, it is not recommended bypassing this pin with a ceramic capacitor > 1nF.
Is it okay to insert only proper resistor (not insert ceramic cap)? or Do you have a recommended value of ceramic cap?
2. About Bootstrap
2-1. the example of calculated Cboot value is 170uF. In the red area, TI selects 1uF capacitor with margin. and 1uF value is about 6 times of 170uF.
Is it okay to multifly 6 times to final Cboot value? or Do you recommend other multiplied value?
If 6 times is okay, do you have any reference document or formula about it?
2-2. Is △VDDA 0.5V right value? (VDD is 15V in customer's application.)
2-3. About applying Ivdd value, It is okay to apply the value in the blue area?
2-4. About bootstrap resistor, I only found the contents below. Where can I fined detailed description for calculating bootstrap resistor? Do you have any reference or application notes?
3. About calculating external resistor of gate pin
3-1. In the example below, it is okay to use the current value in the red box? or should I use different value which is fit to my customer?
3-2. The values of Ron and Roff which are calculated by the formula below is the minimum values that sre not exceeding gate output current. But I think I should consider switching loss, EMI and other variants.
Do you have any reference or application notes about it? (Ron and Roff value considering switching loss, EMI, and other things)
4. About Rgs
In the datasheet, Rgs is typically sized between 5.1k~20kohm and depending on the vth and ratio of Cgd to Cgs of the power devices.
Do you have any reference or application notes for calculating Rgs value?
5. About external Cge
In the datasheet, It is one of the option adding capacitor Cge to prevent problems due to C*dV/dt.
Do you have any reference or application notes for calculating Cge value in the blue box?
6. About INA/INB Input filter
It is okay to use RIN value between 0~100ohm and CIN value between 0~100pF and corner frequency of approximately 100MHz? any other recommendation or specific reference?
Please check these issues. Thanks.
Best regards,
Chase