This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR36510: MARGINING Via FB pin using DAC with I2C

Part Number: LMR36510


Tool/software:

Hi,
I am using LMR36510 for our application. 
Vin = 24V, Vout = 12V, Iout = 0.015mA. 

I need to margin the output voltage via external DAC. May be +30% to -30%. 
Is it possible to do in LMR36510 through Margining DAC (DAC7574IDGS) or else please share the respective Margining DAC part?

Thanks