This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61023: Request for TPS61023 scehamtic review

Part Number: TPS61023


Tool/software:

Hello, 

I need to review my schematic in personal. Is it possible?

The output of TPS61023 is wiered most of the time.

Schematic review required.

thank  you 

  • Hi,

    Lei will reply tomorrow. Thanks.

  • Hi Nabeel,

    Please provide the schematic for review, together with the "wiered behavior" of the output.

    Pay attention that this is a public forum. Just let me know if you have confidential requirement. 

    Regards

    Lei

  • TI DC DC Converter Issue.docx

    Can you check this file, I copied the relevent parts and some information. For your Kind review

  • Hi Nabeel,

    There are three circuits for the TPS61023:

    • VDD3.3V
    • VDD3V3_AA
    • VDD5V

    Do all the three circuits have the same issues? That is, "the output is correct for some time, but again becomes same as input (2.8V) after some time of use".

    Could you capture the waveforms of the Vin, Vout and SW when the devices can work normally? Are there very high SW spikes?

    And also please take a quick experiment: remove the C112, C113 and C108 and try again.

    Regards

    Lei  

  • Hello Lei,

    All circuits have same issue in different cards. The output is same as input and there is no SW waveform.

    At that time I checked the Feeback pin, which has voltage of 1V ~3V (different on different cards). 

    no spikes on SW.

    I checked  C112, C113, C108 for the values 10pF also, but same issue... Also I removed from one IC , but no efect (output same as input). 

    In previous schematic I put 10pF as feedforward capacitor value, but the output capacitance is more that 40uF (it is 50uF for VDD3.3V and VDD3V3_AA /  1100uF for VDD5V to be precise). So I set the Fz=1KHz with these capacitors values. The 1nF feedforward value I set was based on some forums recommendation to use high value for large capacitors. Which I will change again to 220pF as recommended by TI.

    Regards

  • Hi Nabeel,

    We may focus on the TPS61023 for VDD3.3V first.

    Please take a measurement on the Vin, Vout, and SW and inductor current waveforms when the device works at the heaviest load in your application.

    Note that all these Vin, Vout, and SW voltage waveforms should be measured on the device pin.

    And if the procedure from the normal to abnormal behavior can be captured, it will be very helpful! You may try to trigger by the Vout falling.

    Regards

    Lei