This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23755: Change transformer

Part Number: TPS23755

Tool/software:

Hi,

Since there is a need for redesigning due to a new mechanical, we want to reduce the size of the DCDC transformer.

May I ask if the original DCDC transformer model, LDT0950-50, can be replaced with the model PC1312-002SR? Do you have any similar cases? (Inductance change from 150uH to 60uH.)

Thanks!

23755 (1).pdfLDT0950-50_datasheet.pdfPC1312-002SR SPEC Rev_B_20250318.pdf

Jeff

  • Hi Jeff,

    Thanks for reaching out!

    Reducing inductance will cause winder DCM range, PSR could be influenced especially at light load. 

    I would recommended you to double check with Linkcom if PC1312-002SR is suitable for PSR and 250kHz?

    If you need contacts of Linkcom I can loop you in. Thanks!

    Best regards,

    Diang

  • Hi Diang,

    Does transformer vendor know the PD application for PSR and 250kHz?

    And as your descroption, seem not recommend using PC1312-002SR for new design?

    or any other schematic we can adjust for Inductance change from 150uH to 60uH?

    Actually we want reduce the transformer size since reference design LDT0950-50 is big.

    Or you have better suggestion for transformer part number with smaller size?

    Thanks!

    Jeff

  • Hi Jeff,

    Let's check with Linkcom. Thanks!

    Best regards,

    Diang