Other Parts Discussed in Thread: TPS25763-Q1, TS3USB221A-Q1
Tool/software:
I am planning to use the TPS25763-Q1 IC as shown in the diagram below.

In this setup, the laptop or tablet acts as the USB host, and through the TPS25763-Q1 and a MUX, both DP output and USB 3.1 or 3.2 should be routed to a USB hub, allowing connection to various USB devices.
According to the EVM, J29 is UFP only, but I would like to use J30 (USB Type-C) as a UFP to connect to the host, and J29 as a DFP to connect to the hub and access multiple devices.
Is there any way to configure the system to support this data path?