Tool/software:
Vin=12V 2A
Vset=13K
ISET=375R
Battery 3.3V
Why is the VBAT_CHG charging current 50-100mA?
Frank
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Frank,
Given that VIN is 12V, it's possible the device is entering thermal regulation (TREG) and reducing the charge current to prevent overheating.
Could you please test with a lower input voltage, such as 5V, to see if the issue goes away?
Best regards,
Alec
Hi Frank,
Thanks for checking.
I recommend either:
1. Using a buck converter to step down from 12V before supplying VBUS
2. Using a switching charger, which is more efficient than a linear charger at higher input voltages
Due to the nature of the linear topology, power dissipation increases as the voltage drops across the internal FETs and current increases.
Refer to section 8.3.7.6 of the BQ25185 for more details on power dissipation.
Best regards,
Alec