This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25792: NTC Function on TS Pin for BQ25792RQMR and Compatible Fuel Gauge Recommendation for 4S Battery

Part Number: BQ25792
Other Parts Discussed in Thread: BQ40Z50-R2, BQ40Z80, BQ40Z50

Tool/software:

Hi,

I’m working with the BQ25792RQMR battery charger IC, and in my application, I do not require the NTC (temperature sensing) function for battery temperature monitoring. I would like to know:

  1. How can I disable the NTC function on the TS pin?

    • Should I connect the TS pin to REGN or GND directly if not using the NTC feature?

    • Or is there a recommended resistor configuration to safely disable or bypass this function?

  2. Additionally, could you please recommend a suitable fuel gauge IC that is compatible with this charger and supports a 4-cell (4S) Li-Ion battery pack?

Appreciate your guidance. Please respond at your earliest convenience.