Tool/software:
Hello
I'm creating learning data with the Q34Z100, and after fully charging it (FC=1), I let it relax for more than two hours, but VOK did not change from 1 to 0.
upDATE STATUS also did not change from 4 to 5.
I think this is because the learning board's power consumption is high compared to the battery capacity, and the battery voltage changes greatly, but what do you think?
By the way, the battery is 512W and the power consumption of the board is 258mW.