Tool/software:
Hi,
1) Am I correct in understanding that the timing when the BAT terminal reads the voltage is the same as the timing when the VEN pin outputs a voltage?
2) Is it OK if 0V is input to the BAT terminal while no voltage is being output from the VEN terminal?
3) Does the period during which the VEN terminal outputs 2.5V change? It is 1s on the board I created, but it was 20s on the EVM.
4) If I create a circuit like the one below, will the BAT terminal always read a voltage? Could you also check whether there are any problems with the circuit diagram?
Best Regards,
Nishie