Tool/software:
Hi Team,
Could you help to confirm the following questions about TPS63070:
1. During the startup phase, Is the output current capability mainly limited to a typical input current of 1A, as below description, right?

2. On the customer's application, the output voltage is divided into two stages, as below graph
First stage, Vin=3.3V, Vout=3.3V,
Second stage, Vin=3.3V, Vout=7V 1A,
In the second stage, it is controlled by VSEL.
What is the limit current during the Vout=3.3V to Vout=7V process? Is it 3.05~4.105A?