Tool/software:
Hi,
The SNS output is used to indicate system faults. ISNS will go to the predefined level, ISNSFH, when there is a fault.
According to SNS CHARACTERISTICS, when VBB = 6 V to 18 V, ISNSFH = 4mA to 5.3mA, typical 4.5mA.
RISNS Value is 1.3K, so Vsns = 5.2V to 6.89V, and any ADC value above 95% is considered a fault.
When battery voltage is normal, evething is OK.
But when battery voltage is low, Vsns will drop below 5.2V.
Here are two results we measured,.
Vbat=6.9V, Vbb =6.4V, Vsns=4.93V
Vbat=6.5V, Vbb =6.02V, Vsns=4.63V
I think the Isnsfh current source could not supply the same current at low voltage, but didn't find any description in the datasheet.
Could you share your ideas?
Thanks!