Tool/software:
Hi,
My customer had the following questions, would you be able to help assist?
1.) Is it possible to connect two or more channels in parallel to an LED and control them via software, with the goal of generating a higher current (e.g., 250 mA from 2 x 125 mA/channel) for the LED?
2.) Why is the current limit in the LP5861x GUI control set to 50 mA and not 125 mA per channel?
3.) Is there a way to read, adapt, and test the code in the LP586x GUI control? This would help me understand the functionality and parameterization of the LED driver's channels and adapt it to my current project.
Thank you